必須オプションを選択してください
製品詳細
Wiki & 学習
レビュー
PDF をダウンロード

特長

  • The First Official TinyGo + XIAO Starter Kit: TinyGo is a Go compiler specially designed for small places — microcontrollers, WebAssembly, and command-line tools. Co-developed by TinyGo and Seeed Studio, this is the first hardware kit designed specifically for learning embedded development with Go.
  • Comprehensive Tutorials Written by TinyGo Team: The getting-started guide for this kit, hosted at github.com/soypat/seeed-grove, was written specifically for the exact modules included in the box. Every step uses idiomatic Go, real TinyGo driver packages, and code you can immediately read, modify, and extend. 

  • Plug-and-Play, Quick Setup, No Soldering Needed: The kit assembles a carefully selected set of 11 Grove modules alongside the Grove Base for XIAO, covering sensing, display, lighting, and actuation — no soldering, no jumper wires, no breadboards required.
  • XIAO ESP32-C3 Included: Start immediately with the pre-soldered XIAO ESP32-C3, featuring Wi-Fi, Bluetooth LE, and excellent TinyGo support.
  • Fully compatible with Seeed Studio XIAO Family: The kit also supports Seeed Studio XIAO ESP32-S3, XIAO nRF52840(XIAO BLE), XIAO RP2040, XIAO SAMD21, and XIAO RP2350. Simply switch to any other XIAO board at any time using the same Grove Base.

仕様

用途

  • Classroom & Workshop Platform
  • IoT Environmental Monitor
  • Motion Detection & Alert System
  • Touch & Rotary Control Interface
  • Sound-Reactive LED Visualizer

部品リスト

Seeed Studio Grove Base for XIAO - with embedded battery management chipx1
Grove - Piezo Buzzer/Active Buzzer - Arduino/Raspberry Pi Compatiblex1
Grove - Buttonx1
Grove - Sound Sensor Based on LM358 amplifier - Arduino Compatiblex1
Grove - 3-Axis Digital Accelerometerx1
Grove - Touch Sensorx1
Grove - Temperature Sensorx1
Grove - Rotary Angle Sensorx1
Grove - Piezo Vibration Sensorx1
Grove - OLED Display 0.66" (SSD1306)- IIC - 3.3V/5Vx1
Grove - Light Sensor v1.2 - LS06-S Phototransistor Compatible with Arduinox1
Grove - RGB LED Stick (10 - WS2813 Mini 3535) : Full-Color RGB LED Lightingx1

FAQ

Yes. The solder-free setup, consistent hardware, and openly licensed tutorial content make this kit well suited for university courses, embedded Go workshops, and maker club sessions.
Two repositories cover this kit: • Grove module tutorial & drivers: github.com/soypat/seeed-grove • Wireless & ESP32 examples (official TinyGo): https://tinygo.org/docs/reference/microcontrollers/ For TinyGo language questions, visit tinygo.org or join #tinygo in the Gophers Slack. For Grove hardware documentation, visit wiki.seeedstudio.com.
As of TinyGo v0.41, the XIAO ESP32-C3 is a TinyGo Featured Board, with native Wi-Fi via the espradio package and direct flashing via espflasher. It offers the best balance of TinyGo support, built-in wireless, compact size, and value, making it the ideal starting point. You can switch to other compatible XIAO boards.
Basic Go familiarity is helpful but not required. The tutorials introduce hardware and language concepts side by side. The TinyGo Playground (play.tinygo.org) also lets you experiment with TinyGo in your browser before connecting any hardware.
TinyGo is an open-source Go compiler based on LLVM, designed for microcontrollers and WebAssembly. It supports over 150 development boards and brings complete Go — static typing, goroutines, channels, and the standard library — to embedded systems. Learn more at tinygo.org.
All 11 modules connect via plug-and-play Grove 4-pin connectors — no soldering, no breadboarding, no wiring diagrams. The official TinyGo tutorial starts from zero and builds progressively. If you can write basic Go code, you have everything you need to get started.

TinyGo Starter Kit with Seeed Studio XIAO - Program Embedded Hardware in Go, Solderless, Grove Modules, Official TinyGo Tutorial

SKU E26072201
Start programming embedded hardware in Go with everything you need in one box. This TinyGo Starter Kit with Seeed Studio XIAO combines a pre-soldered XIAO ESP32-C3, Grove Base for XIAO, 11 plug-and-play Grove modules covering sensing, actuation, display, and lighting, together with an official getting-started tutorial series developed by the TinyGo team. Launched through a collaboration between Seeed Studio and TinyGo, this kit is designed for Go developers and beginners alike to quickly get started programming embedded hardware in Go, and then proceed to build real, portable projects with XIAO.
XIAO Starter KitXIAOML KitGrove Beginner Kit for Arduino
JPY¥7546.00
Seeeduino XIAO用Grove シールド バッテリー管理チップ 搭載 - Grove Shield for Seeeduino XIAO - with Embedded Battery Management Chipx1¥618.00
Grove 光センサー v1.2 - Grove Light Sensorx1¥315.00
Grove - Piezo Vibration Sensorx1¥1093.00
Grove 温度センサ - Grove Temperature Sensorx1¥436.00
Grove 回転角センサ - Grove Rotary Angle Sensorx1¥507.00
Grove ブザー - Grove Buzzerx1¥301.00
Grove 音センサ - Grove Sound Sensorx1¥855.00
Grove - Touch Sensorx1¥681.00
Grove ボタン - Grove Buttonx1¥301.00
Grove RGB LED スティック (10-WS2813 Mini) Arduino/Raspberry Pi用x1¥855.00
Grove - 3-Axis Digital Accelerometer (LIS3DHTR)x1¥713.00
Grove - OLED Display 0.66" (SSD1306)- IIC - 3.3V/5Vx1¥871.00
必須オプションを選択してください
  • Free Insurance Included On Us
  • Flexible Payments with PayPal Pay Later
  • Avoid Import Fees: Ship Tax-Free from Local Warehouses
  • 1 on 1 Support | 12-Month Warranty | 30-Day Return Policy